Technical FAQs

Ask a Question

What is the field install kit for auxiliary contacts on the GJL mechanism of a 8539 starter? <br /><br />

We do not offer externally mounted auxiliary contacts for a GJL mechanism. Customer will have to use the GJL internally mounted auxiliary contact which is Catalog # AAC. It has form C contacts that will change state when the breaker trips or is turned on or off.

CTA-ID : 2048861
Was this helpful?
What can we do to improve the information ?