Technical FAQs

Ask a Question

What is the NEMA rating or IP degree of protection for the door-mounted 32598 RE12 and 32600 RE22 rotary handle operator for the Powerpact D frame (and NSJ) breaker?

32598 and 32600 are IEC-Style Door-Mounted Rotary Operating Handles. The handle mechanism can be used in NEMA 3R and 12 enclosure applications. Degree of protection: IP40 as per IEC 529..

CTA-ID : 2049024
Was this helpful?
What can we do to improve the information ?