Technical FAQs

Ask a Question

What bus bar material is used in the PAK Construction Site and Recreational Vehicle Park Panels?

Both plated copper and plated aluminum current carrying parts are used. An option for all copper is not available.

CTA-ID : 2049113
Was this helpful?
What can we do to improve the information ?