Technical FAQs

Ask a Question

What is the Powerpact P frame circuit breaker mounting depth when the door mounted rotary operating handle is included with the breaker?

This Powerpact P frame circuit breaker will have a suffix of RE10 for a standard black handle or an RE16 for a red handle on yellow bezel. The minimum mounting depth of the circuit breaker is 8.9 inches and the maximum mounting depth is 23.8 inches.


CTA-ID : 2049042
Was this helpful?
What can we do to improve the information ?