Technical FAQs

Ask a Question

Is it possible to order an I-Line II circuit breaker type busplug with ground fault capability?

Issue:
Is it possible to order an I-Line II circuit breaker type busplug with ground fault capability?   

Product Line:
I Line busway.

Environment:
Products sold in the United States.

Cause:
Product selection.

Resolution:
Yes. A bus plug with ground fault features is processed as a special device. A ground fault modual is added inside the bus plug enclosure for bus plug amperages 250 amps and below. For amperages above 250 amps, the circuit breaker that is provided with the standard bus plug is replaced with a circuit breaker with gound fault features.


CTA-ID : 2049027
Was this helpful?
What can we do to improve the information ?