Technical FAQs

Ask a Question

Are the MD50 Motor Disconnects rated for use with DC voltage?

The MD50 Motor Disconnects are rated only for AC voltage applications.


CTA-ID : 2049038
Was this helpful?
What can we do to improve the information ?