Technical FAQs

Ask a Question

What are the dimensions of the 9001BW146?

Customer was advised the same basic enclosure is use as for the two button but only one hole is provided (the bottom hole). Dimensions are 4.25``H x 2.76``W x 3.60``D


CTA-ID : 2048848
Was this helpful?
What can we do to improve the information ?