Technical FAQs

Ask a Question

Can a QB I-Line breaker be used in an NH1B interior that currently contains FA and Q2 branch breakers?<br /><br />



Issue:
Selection of replacement circuit breakers for the obsolete NH1B panelboards.

Product Line:
Obsolete NH1B panelboards.

Environment:
NH1B panelboards, formerly sold and supported in the USA.

Cause:
Availability of branch circuit breakers for the obsolete NH1B circuit breaker panelboards.

Resolution:
The maximum branch breaker the NH1B panel was designed to accept was the F frame 100A ( FAL type 50A max for column width) breaker. The Q2 and the QB 225A frame breakers may fit however, neither the Q2 nor the QB branch breakers have been tested or evaluated for use in the NH1B interiors. Also, keep in mind the maximum ampere rating of a branch breaker for a NH1B panel is still 100A even if they decide to use the QB 225A frame breaker which are not suppose to be in that panel.







 
Was this helpful?
What can we do to improve the information ?