Technical FAQs

Ask a Question

What are the dimensions for the J250R circuit breaker enclosure?

Issue:
Dimension

Product Line:
Circuit Breaker Enclosure

Cause:
Dimensions

Resolution:
This enclosure is 31.28" H x 14.64" W x 6.2" D. Click this link to access the Approval Drawing #3364S.
http://static.schneider-electric.us/docs/Circuit%20Protection/Circuit%20Breaker%20Enclosures/3364S.pdf

The drawing is also attached. 


CTA-ID : 2049173
Was this helpful?
What can we do to improve the information ?