Technical FAQs

Ask a Question

<br />What do the forms on a 9007C54B Form D5, T, Y35, and Y140 mean ?<br />

This is a special configuration for Chrysler per the Y35 . The D5 is for a 5 pin microconnector, T is for tamper proof screws, (both of which are exclusive to the Y35 for Chrysler) and Y140 for a Viton seal. The Y140 is the only form that can be added to other 9007C type switches.

CTA-ID : 2049054
Was this helpful?
What can we do to improve the information ?