Technical FAQs

Ask a Question

Do we offer an option for a UL C62 lightning arresting for any of our NQ,NF,or I-line panels?

We have the SDSA3650 and the SDSA1175 devices but they are not part of the product selector and will need to be added as a special and priced per Digest page 9-37 in the Digest 174. This device does NOT meet the TVSS UL1449 specifications. If both ULC62 and UL1449 specifications are required then both a TVSS unit and the SDSA devices will need to be selected. The TVSS unit is available in product selectors.


CTA-ID : 2049260
Was this helpful?
What can we do to improve the information ?