Technical FAQs

Ask a Question

<br />Can I-line II busway be used for AC or DC applications?

Yes. It can be used with AC or DC voltages (600 volt max).


CTA-ID : 2048952
Was this helpful?
What can we do to improve the information ?