Technical FAQs

Ask a Question

Are the Class 8940 pump panels available in NEMA 4/4X enclosures?

No, these panels are only available in NEMA 3R enclosures.


CTA-ID : 2049074
Was this helpful?
What can we do to improve the information ?