Technical FAQs

Ask a Question

What are the differences between FCA1 and FCA1A?<br />

FCA1 was designed in Italy and the FCA1A was designed in the USA. The FCA1A is heavier. Both are shrouds for the FAL or FHL Frame Breaker. Order FCA1A.

CTA-ID : 2048858
Was this helpful?
What can we do to improve the information ?