Technical FAQs

Ask a Question

Can a key interlock be factory installed on a P1200S circuit breaker enclosure?

Issue:
Product Design Features

Product Line:
Circuit Breaker Enclosures

Environment:
Accessories

Cause:
Application

Resolution:

A key interlock cannot be factory installed on a P1200S enclosure. However, we can provide a key interlock on a P1200AWK enclosure, which you may want to consider. We would provide the P frame PowerPact circuit breaker, the P1200AWK circuit breaker enclosure and key interlock all factory assembled. The catalog number would be dependent upon the circuit breaker required.


CTA-ID : 2049148
Was this helpful?
What can we do to improve the information ?