Technical FAQs

Ask a Question

What Class of fuse does the H361CS safety switch accept?

This switch accepts Class H or K fuses as standard. Options include Class R fuses (field install Class R Fuse Kit) and Class J fuses (field relocate the fuse base assembly to alternate position marked in the enclosure). With Class H or K fuses installed, the switch is UL listed for use on systems with up to 10,000 RMS Symmetrical Amperes available fault current. With Class R fuses (and Class R Fuse Kit installed) or Class J fuses installed, the switch is UL listed for use on systems with up to 200,000 RMS Symmetrical Amperes available fault current.
NOTE: DO NOT USE RENEWABLE LINK FUSES IN SQUARE D SAFETY SWITCHES. The use of renewable link fuses may adversely affect user safety, impair reliability and will void the warranty.


CTA-ID : 2048935
Was this helpful?
What can we do to improve the information ?