Technical FAQs

Ask a Question

Can a shunt trip accessory be added to an EZM11600CB?

Issue:
Product design features

Product Line:
EZM Metering

Environment:
Shunt Trip

Cause;
Application

Resolution:
Yes. The main breaker used is the PAF2026. The PA11021 shunt trip accessory can be field installed into the circuit breaker. This shunt trip module is suitable for 120, 208 or 240 Vac. Other shunt trip modules available are PA11042 (24 Vac), PA11086 (208 or 480 Vac), PA11027 (24 Vdc), PA11028 (48 Vdc), PA11029 (125 Vdc) and PA11030 (250 Vdc).


CTA-ID : 2048868
Was this helpful?
What can we do to improve the information ?