Technical FAQs

Ask a Question

What is the tolerance or voltage range for Definite Purpose 8910DPA coils?

The coils are designed to operate at a range of -15% to +10% of nominal.


CTA-ID : 2049258
Was this helpful?
What can we do to improve the information ?