Technical FAQs

Ask a Question

What is the wire range for the lugs on a URTRS101B?

The Line/Load/Neutral lugs wire range is #8 to #2/0 AWG (Al/Cu).


CTA-ID : 2049250
Was this helpful?
What can we do to improve the information ?