Technical FAQs

Ask a Question

Can the EZMK312400 (3-Phase IN - 1-Phase OUT) branch units be converted in the field to an EZMK332400 (3-Phase IN and 3Phase OUT)?

Issue:
Product Design features

Product Line:
EZM metering equipment

Environment:
Meter socket conversion

Cause:
Utility approval

Resolution:
No., The EZM branch devices that are 3-Phase IN - 1-Phase OUT CANNOT be converted in the field to 3-Phase IN - 3Phase OUT. Also, EZM branch devices that are 3-Phase IN - 3-Phase OUT, CANNOT be converted in the field to 3-Phase IN - 1-Phase OUT. The correct branch device for the voltage system both IN and OUT MUST be obtained from the factory. 


CTA-ID : 2048904
Was this helpful?
What can we do to improve the information ?