Technical FAQs

Ask a Question

Can the 9012G pressure switch be used to activate an alarm on low pressure.

Yes. This switch has Single Pole Double Throw contacts (at least 1-N/O and 1-N/C contacts). The alarm will begin when the pressure falls to the decreasing pressure set point and continue until the pressure rises to the increasing pressure set point where it goes out.


CTA-ID : 2049008
Was this helpful?
What can we do to improve the information ?