Technical FAQs

Ask a Question

What are the differences between a 9070 Type T and Type EO Industrial Control Power Transformers?

Issue:
9070 Type EO vs Type T

Product Line:
LV Transformers

Environment:
Applies to Industrial Control Transformers by SquareD/Schneider Electric

Cause:
Industrial Control Transformers offered in different types

Resolution:

The 9070 Type T is the current, standard design. It has accessories, both factory or field installed, available (fuse blocks, fingersafe covers, fuse pullers). The EO is part of an older design offering which supplies better regulation. There are no accessories available for type EO and many designs are of limited availability .


CTA-ID : 2048917
Was this helpful?
What can we do to improve the information ?