Technical FAQs

Ask a Question

What is the solid neutral assembly for use with a P1200S circuit breaker enclosure?

Issue:
Selection

Product Line:
Circuit Breaker Enclosure

Cause:
Selection

Resolution:
Use SN1200. For an application using a P-Frame PowerPact breaker with integral ground fault protection, use S33576MK (Neutral Assembly) and S33576 (Neutral Current Transformer) (400 - 1200A).


CTA-ID : 2048892
Was this helpful?
What can we do to improve the information ?