Technical FAQs

Ask a Question

HPALI is that a fixed padlock attachment?

Yes. Two tamper-resistant screws are used to attach it. to the breaker.


CTA-ID : 2049129
Was this helpful?
What can we do to improve the information ?