Technical FAQs

Ask a Question

Can a 225A subfeed lug kit (SL225) be installed in a HCN I-line panel?

Issue:
Can a 225A subfeed lug kit (SL225) be installed in a HCN I-line panel?

Product Line:
Panelboards

Environment:
I-Line HCN

Cause:
Availability

Resolution:
No. The maximum subfeed lug kit that can be installed in an HCN panel is an SL100 which is rated 100A.


CTA-ID : 2048934

Was this helpful?
What can we do to improve the information ?