Technical FAQs

Ask a Question

At what percentage of nominal voltage will the powerpact H and J frame shunt trip operate?

The shunt trip will trip the circuit breaker when the control voltage applied to the shunt trip rises above 70% of the shunt trips rated voltage.


CTA-ID : 2049542
Was this helpful?
What can we do to improve the information ?