Technical FAQs

Ask a Question

What are the dimensions for an HU364?

An HU364 is 29`` H x 17.13`` W x 8.25`` D. The width, including the external operating handle, is 18.5``.


CTA-ID : 2049414
Was this helpful?
What can we do to improve the information ?