Technical FAQs

Ask a Question

Does the GS1DU3 meet NFPA 79 applications?

Yes, with the addition of the GS1AD010 handle it will meet the NFPA 79 application.


CTA-ID : 2048832
Was this helpful?
What can we do to improve the information ?