Technical FAQs

Ask a Question

What is minimum and maximum distance from the back of the breaker to the door, that the RE10 and RE16 Operating mechs can be used with?<br />

The minimum enclosure depth would need to be 8.9`` and the maximum depth it can be is 23.8``

CTA-ID : 2048901
Was this helpful?
What can we do to improve the information ?