Technical FAQs

Ask a Question

Can an EZML312400 (3phase in - 1phase out branch device), connect with an EZM11600TB 1 phase main device.

NO.... The 3-Phase horizontal cross bus in an EZML312400 branch device WILL NOT connect to the 1-Phase horizontal cross bus as used in an EZM11600TB.
This is a product markings issue having to do with the UL Listing of these Modular-Panelboard Cabinets.

CTA-ID : 2048903
Was this helpful?
What can we do to improve the information ?