Technical FAQs

Ask a Question

Is there a retaining clip for the Q12100TF main breaker used in the QO8-16M, Series L7, load center?

Issue:
Selection

Product Line:
Obsolete QO Load Center

Cause:
Selection

Resolution:
There is no need for a retaining clip, as the Q12100TF was not a back-fed main. Also, the Q2100TF circuit breaker is `Obsolete`, with no replacement.


CTA-ID : 2049191
Was this helpful?
What can we do to improve the information ?