Technical FAQs

Ask a Question

Can a key interlock be factory installed on the P-Frame, P1200R, P1200S or P1200AWK, circuit breaker enclosures?

Issue:
Product Design Features

Product Line:
Circuit Breaker Enclosures

Environment:
Accessories

Cause:
Application

Resolution:

A key interlock CANNOT be factory installed on the P1200R or P1200S enclosures. However, a Key Interlock can be provided on the P1200AWK enclosure. The P1200AWK also carries a NEMA 3R rating, by removing the drain screw in the bottom endwall. The factory would provide the P frame PowerPact circuit breaker, the P1200AWK circuit breaker enclosure and key interlock all factory assembled. The catalog number would be dependent upon the circuit breaker required.

 
Was this helpful?
What can we do to improve the information ?