Technical FAQs

Ask a Question

Can a 9001K3 mechanical interlock be used with illuminated operators?

Yes. This type of interlock can be used with illuminated operators, as the mechanism works with the contact blocks only. It will require extra depth in the enclosure, however.


CTA-ID : 2049112
Was this helpful?
What can we do to improve the information ?