Technical FAQs

Ask a Question

What are the part numbers for jumpers for the AB1VV635U?

AB1AL6 is an 80 point non-insulated jumper, AB1ALN62 is a 2 point insulated jumper, and AB1ALN610 is a 10 point insulated jumper. All are available as a standard package of (10).

CTA-ID : 2049826
Was this helpful?
What can we do to improve the information ?