Technical FAQs

Ask a Question

Are the new 60 circuit HOMELINE load centers UL Listed?

Yes, they are UL Listed, File #E6294.


CTA-ID : 2049820
Was this helpful?
What can we do to improve the information ?