Technical FAQs

Ask a Question

Does Square D offer any QO or Homeline load centers with more than 42 spaces(and or circuits)?

Issue:
Product Offering

Product Line:
QO load centers

Environment:
Maximum spaces/circuits

Cause:
Application

Resolution:
Yes, with the elimination of the "42 circuit rule" (2005 National Electrical Code (NEC) Article 408.35), applicable to a panel defined as a lighting and appliance panelboard. The QO and HOMELINE product lines have been expanded to provide more than 42 circuits. Please refer to the current Schneider Electric Digest, Section 1, for the current product catalog numbers.
Link to online Digest:
http://www.digestplus-us.schneider-electric.com/

NOTE: The new QO Plug-On Neutral load centers are available up to 60 full spaces(NO tandems) maximum. The Homeline Plug-On Neutral load centers are available up to 60 full spaces(120 circuits with tandems) maximum.



CTA-ID : 2049792
Was this helpful?
What can we do to improve the information ?