Technical FAQs

Ask a Question

VCF5: What is the IP rating of this switch?

The switch itself is rated IP20, the handle is rated IP65 ( handle gasket is included and would have to be used.)


CTA-ID : 2049793
Was this helpful?
What can we do to improve the information ?