Technical FAQs

Ask a Question

9007 Type L140 cable pulls - are they Class 1 Div 2 rated? Are they hermetically sealed?<br /><br />

L140`s are not rated for Class 1 Div 2; do not offer hermetically sealed contacts for these.

CTA-ID : 2049771
Was this helpful?
What can we do to improve the information ?