Technical FAQs

Ask a Question

Can a resin transformer, enclosure style A, style B, and style C be mounted on it`s back (vertically( with the wiring compartment in the front for an indoor application?

Vertical mounting of a sealed resin transformer is acceptable as long as the wiring compartment is even with or lower than the top of the transformer. The NEMA 3R rating of the transformer is not maintained when the transformer is mounted in a non-vertical orientation.


CTA-ID : 2049690
Was this helpful?
What can we do to improve the information ?