Technical FAQs

Ask a Question

When is a retaining kit needed in a loadcenter?<br /><br /><br />

Per code, retaining kits are needed if a branch breaker will be used as a main breaker in the panelboard it resides in. Retaining kits are NOT required for branch breakers that are used as main breaker for another panelboard.

CTA-ID : 2049671
Was this helpful?
What can we do to improve the information ?