Technical FAQs

Ask a Question

Is there a delay before the contacts change state on a 8430MPD phase failure relay?

The delay on pick up is 0.1 seconds and the delay on drop out is a maximum of 3 seconds. This is non-adjustable.

CTA-ID : 2049637
Was this helpful?
What can we do to improve the information ?