Technical FAQs

Ask a Question

9007AW16 is single pole double throw limit switch - does it have isolated contacts?<br /><br />

No. Isolated contacts depend on how far apart the poles are, electrical gap may not be far enough apart. 9007AW16 does not have isolated contacts, the source must be same for both circuits. Would have to go with 9007AW18, to get isolated contacts. In this case, each NO/NC pair must have the same polarity, but the two circuit pairs could be wired as isolated from each other.

CTA-ID : 2049762
Was this helpful?
What can we do to improve the information ?