Technical FAQs

Ask a Question

Can the drive be used as a frequency converter instead of on a motor?<br />

This type of application is not good nor recommended for use of a drive because the drive will shift voltage and frequency as loading on the output of the drive changes. The unit is not a true constant v/hz producer to be used as a pure frequency converter in this fashion without a load present.

CTA-ID : 2049780
Was this helpful?
What can we do to improve the information ?