Technical FAQs

Ask a Question

What is the arc suppressor assembly for the 9422 TCF33 disconnect switch ?

This switch utilizes a one-piece arc suppressor assembly. It is part number 40566-355-50. This piece comes without the nameplate; the nameplate is not available.

CTA-ID : 2049206
Was this helpful?
What can we do to improve the information ?