Technical FAQs

Ask a Question

What are the features provided with circuit breaker suffix 2200?`

This is the combination of the 1021 shunt trip and the 2100 alarm switch.


CTA-ID : 2049589
Was this helpful?
What can we do to improve the information ?