Technical FAQs

Ask a Question

What is the quantity and size of wire that can be terminated on the SN0310 Neutral Assembly?

Issue:
Product Features

Product Line:
Double Throw Safety Switch

Cause:
Clarification of wire range

Resolution:
The SN0310 Neutral Assembly is provided with (3) lugs with a wire range of #14 - 1/0 AL/CU for the incoming and outgoing neutrals and (2) lugs with a wire range of #14 - 6 AL/CU for the service ground(s).

CTA-ID : 2049028
Was this helpful?
What can we do to improve the information ?