Technical FAQs

Ask a Question

9007C has 10 degree pretravel, book says 13 degrees with reed contacts<br /><br />

``The head, 9007C is configured for 10 degrees pretravel and is manufactured to that standard. When using it on a reed switch, the contact operating mechanism does not allow precharging, so that the reed switch requires an additional 2 to 3 degrees of pretravel before contacts change state. Thus, the head is manufactured to a 10 degree standard, as the customer found stamped on the head. The total configuration meets the published standard as was noted in the Digest. ``

CTA-ID : 2049772
Was this helpful?
What can we do to improve the information ?