Technical FAQs

Ask a Question

Are the UL 489 C60N breakers (120/240 Vac) DC rated as well?

The ``C`` curve is rated for 60VDC for single pole breaker and 125VDC for 2pole breakers. ``D`` curve breakers are not DC voltage rated.


CTA-ID : 2048963
Was this helpful?
What can we do to improve the information ?