Technical FAQs

Ask a Question

What is the Catalog Number for a 225 amp combination service entrance device that has CT provisions for use with Photovoltaic system applications?

Current product design

Product Line:
Combination Service Entrance Devices

CT provisions for use with on PV applications


The Square D CSED that has CT provisions for Photovoltaic system applications is catalog number SC2636M225FPV. 

NOTE: This device is a Standard CSED, that is 225amp Max., Main Breaker, Ring type, 26spaces-36circuit using tandems, but has provisions to install CTs between the Main Breaker and the Load Center interior to allow for monitoring usage in a Photovoltaic Application.

CTA-ID : 2049579
Was this helpful?
What can we do to improve the information ?