Technical FAQs

Ask a Question

Can ground fault equipment protection be provided with an LUS U-Line starter ?

No . Use instead a LUB** self-protected base with a LUCM multi-function control unit ( which includes this as a built-in function) .


CTA-ID : 2049553
Was this helpful?
What can we do to improve the information ?